JacTone PVSTOP Solar Panel Block Outs is only available to buy in quantities of 1
Product Information
PVSTOP is the only known solution for ‘switching off’ solar panels, making them safe in the event of a short circuit or emergency incidents such as a fire, flood or storm. PVSTOP does this by acting as a liquid blanket that is sprayed onto the solar panel and blocking out the light – the energy source.
The world is in the midst of a clean energy revolution driven largely by rising grid electricity prices, government incentive schemes and positive public sentiment toward protecting the future of our planet. The increasing uptake of solar panels and the downward pressure on solar PV system pricing has led to an unprecedented level of growth in the global solar PV system market, growth that is forecast to increase exponentially in the decades ahead. In line with the exponential growth of the solar industry, there has been a similar growth in the number of fire and emergency related incidents involving solar PV systems, highlighting several unanticipated safety risks.