1. Accuracy/Concentricity:
Holders should be selected based on their ability to hold the tool concentric to spindle rotation. ER collet holders lend themselves to universal applications, light milling and drilling. They are the low-cost solution for many SME’s, due to their versatility - and could achieve a 10-micron run out with a precision collet. The Toolholder with the best accuracy are Shrink / Hydraulic holders, which can achieve a higher clamping force for heavier high-speed machining and an accuracy of 3-micron runout.
2. Balance:
As you increase your spindle speeds, it becomes more important to take note of the balance of the holder. ER collets tend to be balanced to 12,000rpm 6.8G and Shrink/ Hydraulic holders 25,000rpm 2.5G. The effect that a lack of balance has on your cutting operation is poor tool life and poor surface finish. Many Cutting tool manufacturers produce cutting tools which are balanced by design - meaning when a tool is put into a Toolholder, the whole unit stays balanced. We see balance as an issue when your RPM of the spindle is over 12,000 rpm. Machining higher than this could result in spindle vibration and damage to your machine spindle with balancing. (Think car tyres… just like a car tyre needs to be balanced, so does a Toolholder). A balancing machine is available to balance your Toolholders.