In our previous blog, we explored the different types of Toolholders, so now we’re going to take you through a more in-depth, specific comparison of Heat Shrink vs Hydraulic Toolholders.
So first, a quick recap of the fact sheets for both:
Our Applications Engineers say…
The Hydraulic vs Heat Shrink debate has been around for a long time, and there are pros and cons with each.
You can see from the fact sheets above the benefits of using each type of Toolholder within various applications.
Hopefully, you’re finding this information useful, because something we see regularly on-site with customers is a preference to buy cheaper Collets, but the customer not understand why they are struggling to hold tolerances.
If you need access to sidewalls and versatility when 5-axis machining, the Heat Shrink Toolholder will perform much better at this than the Hydraulic.
Why? The Heat Shrink is much more streamlined in its’ external bore dimensions (OD). The hydraulic system in the Hydraulic Toolholder on the other hand takes up a lot more space, meaning the Toolholder is less streamlined.
As well as matching to your machining applications, it is worth considering an overall cost comparison too.
To use Heat Shrink Toolholders you’ll need to purchase a Heat Shrink machine, whereas when using Hydraulic you don’t, but the Toolholders themselves are much more expensive to purchase.
Some companies may cut corners and use blow torches to try to replicate the effect of using a Heat Shrink Toolholder, but the inconsistency of heat going into the holder changes the stresses of the material in the holder and causes the toolholders life to deteriorate faster. We’d advise against this.
Using a Heat Shrink machine and Toolholders will ensure the same performance every time.
However, it’s important to understand how to use the Heat Shrink machine properly, giving enough time between reheating for your Toolholders to cool down. Not doing so will destroy the holder, and you may struggle to get tools in and out too!
When using Hydraulic Toolholders it is a lot quicker to change tools over, simply loosen the clamping screw.
Finally, we’ve seen many a customer attempt to Heat Shrink a Hydraulic toolholder and the results aren’t good!
That’s why it’s worth taking the time to understand what you’re working with and why, and we hope these blogs have helped you on your way to doing that.