Grinders and grinder tools really are essential power tools used across a multitude of industries - ranging from metal fabrication jobs and construction to DIY home improvement projects and more. So whether you are cutting, grinding, or polishing, the right grinder tool can make your work faster, easier, and more precise... Read more below.
Definition: Grinder tools are power tools that are used for cutting, grinding, and polishing various materials like metal, stone, or wood. They use rotating cutting discs / disc cutters or wheels, usually made from abrasive materials, to remove unwanted parts of a surface or to shape and smooth it. As a result, Grinders come in different types, such as brushless angle grinders, bench grinders, and die grinders, each designed for specific tasks. As a result, these tools are commonly used in construction, metalworking, and DIY projects because they make it easier and faster to prepare, shape, or finish surfaces.
Some grinders are also handheld for better control, while others are larger and mounted on a stand or table for heavier tasks. Grinders can be corded, connecting directly to an electrical socket, or cordless, powered by rechargeable batteries, making them convenient for use in places without easy access to power as well.
How to Choose the Correct Grinder For You?
Grinders and grinder tools really are essential power tools used across a multitude of industries - ranging from metal fabrication jobs and construction to DIY home improvement projects and more.
So whether you are cutting, grinding, or polishing, the right grinder tool can make your work faster, easier, and more precise as a result.
But, how do you choose the right one for you?
Well, good news, we have put together this comprehensive guide to grinders, which will help us delve into the world of grinder tools and the range of angle grinders available. Consequently, this guide will explore the different types available to you, covering their applications, key components, and safety aspects that make these tools indispensable for both professionals and hobbyists alike.
Grinders are very adaptable power tools that are designed for material removal tasks, primarily through the use of abrasive cutting discs or grinding wheels, and date back to the mid 1950's.
Consequently, these machines have evolved significantly over the years since then, offering you a lot more enhanced precision, speed, and efficiency in various cutting, grinding, and polishing tasks these days, then when they first came out.
Industries Grinders Are Ideal For
As a result, the importance that grinders play today really cannot be overstated. For instance, they play a key role in numerous industries, from construction and metalworking to precision engineering and even home DIY projects.
So, whether you are smoothing welds, cutting through tough materials, or finishing surfaces to a high polish, grinders offer you the ability to do so.
Consequently, some of these consist of:
Construction
Grinders are used for cutting materials like metal, tile, and concrete, as well as for smoothing surfaces and preparing edges, making them essential tools in construction projects.
Metalworking
In metalworking, grinders really are key for shaping, grinding, and polishing metals in tasks like welding prep and finishing metal parts, ensuring high precision and smooth finishes.
Automotive
Grinders are also commonly used in automotive work for grinding, polishing, and removing rust or old paint on vehicle parts and for carrying out precise metalwork in repairs and restoration.
Manufacturing
In manufacturing, grinders are often used for machining, shaping, and finishing metal components or equipment parts, making them ideally placed in production processes.
Woodworking
Grinders serve woodworking uses by helping you with sanding, smoothing edges, shaping wood, and sharpening tools, which help you to achieve fine, detailed finishes on your wood projects as a result.
Shipbuilding
Shipbuilders rely heavily on grinders for cutting and welding prep, grinding down welds, and removing corrosion in ship maintenance and construction work.
Aerospace
In aerospace, grinders are used to precisely shape and polish materials, especially metals, while adhering to high safety and quality standards for aviation components.
Railway Maintenance
Grinders are also used in railway maintenance for rail repair, smoothing welds, and ensuring track surfaces are even and safe for trains, contributing to track reliability.
Stone and Masonry
Grinders are also ideal for cutting and polishing stone, concrete, and bricks, especially in tasks like wall chasing and masonry, where durability and precision really are needed.
Plumbing and HVAC
In plumbing and HVAC work, grinders are also used for cutting pipes, smoothing edges, and preparing materials for fittings and installations - making the setup a lot more efficient as a result.
Grinder Tools Application Uses
As you can see, grinder tools are used in many industries, and this is in part thanks to their application uses.
For instance, here they are suitable for:
Cutting Metal
Grinders are frequently used to cut through metal sheets, bars, and rods, making them essential for fabrication and construction projects that require precise cuts.
Smoothing Welds
After welding, grinders smooth down rough welds, creating a clean finish. This is especially useful in metalworking and automotive industries for professional-looking results.
Removing Rust and Paint
Grinders with abrasive discs are effective at removing rust, old paint, and corrosion from metal surfaces, which is important for restoration and prep work.
Sharpening Tools
Bench grinders are often used to sharpen tools such as chisels, drill bits, and blades, keeping them effective and extending their lifespan.
Polishing Surfaces
With polishing attachments, grinders can bring surfaces to a high shine, making them ideal for finishing work in metal fabrication and automotive detailing.
Cutting Tile and Stone
Grinders with diamond blades can cut through tile, stone, and concrete, making them useful for tiling, masonry, and other construction applications.
Surface Preparation
Before painting or coating, grinders are used to prepare surfaces by removing rough spots or smoothing areas, ensuring better adherence and a professional finish.
Grinding Excess Material
Heavy-duty grinders remove excess material from large workpieces, which is essential in fabrication processes to achieve desired shapes and dimensions.
Engraving and Detailing
Die grinders and rotary tools are perfect for engraving, carving, and adding intricate details to metal, wood, or stone surfaces, useful in crafting and metalwork.
Grooving and Channeling
Grinders, such as wall chasers, are used to create channels or grooves in walls or floors for wiring or plumbing installations, often needed in construction and renovation.
Types of Grinders Available
There are numerous types of grinders available, each designed for specific applications and different tasks.
For instance, these can consist of:
Angle Grinders
Perhaps the most well-known type of grinder, angle grinders, are handheld tools used for cutting, grinding, and polishing.
Consequently, they come in various sizes, with different disc diameters to suit different tasks as well.
For instance, angle grinders are commonly used in construction and metalworking, with brands like Makita angle grinders and DeWALT grinders, which are popular choices among professionals, especially due to the reliability these brands have become well known for.
Angle grinders can also be either corded or cordless.
Corded Angle Grinders
Corded angle grinders, such as the Angle Grinder 240V, provide you with consistent power and are ideal for heavy-duty tasks especially.
Cordless Grinders
Cordless grinders, like the Brushless Cordless Angle Grinder with 18V XR XR Brushless Cordless technology, offer you greater mobility and convenience, especially in areas without easy access to power outlets.
Bench Grinders
Typically used for sharpening hand tools and other rough grinding tasks, bench grinders are mounted on a bench or pedestal.
Consequently, they feature two wheels of different grit sizes, allowing for both coarse and fine grinding to then occur easily.
Bench grinders really are a staple in workshops and are essential for maintaining the sharpness of tools as well.
Die Grinders
A smaller, more precise tool, die grinders are often used in more intricate metalwork, including engraving and smoothing out tight spaces.
Air die grinders, powered by air compressers, are common in automotive and metal fabrication jobs - due to their high speed and precision they can give you.
Belt Grinders
Ideal for large-scale material removal and finishing, belt grinders then use a sanding belt rather than a grinding wheel.
As a result, they are commonly found in industrial settings and are excellent for grinding flat surfaces or removing excess material quickly.
Straight Grinders
Similar to die grinders but larger, straight grinders are used for heavier-duty grinding applications.
This makes them ideal for tasks that require a powerful and precise tool to grind down surfaces or remove welds for instance.
Surface Grinders
These grinders are then used to produce a smooth finish on flat surfaces.
For instance, surface grinding is widely used in precision engineering and machining, where a high degree of accuracy is required.
Cylindrical Grinders
These are specialised grinders used to shape the outer surface of a cylindrical object, and are highly effective in manufacturing and automotive industries for tasks that require extreme precision.
Key Components and Features of Grinders
Each grinder tool consists of several key components that contribute to its performance and give you more features for certain tasks.
For instance, some of the more important and common ones consist of:
Grinding Wheel or Disc
The abrasive wheel or cutting disc is the part that does the actual cutting or grinding and attaches to the Angle Grinder Body.
These can then come in various materials like aluminium oxide, silicon carbide, or diamond-tipped for use with different tasks.
Consequently, choosing the right cutting disc or grinding wheel is really key for the efficiency and safety of the tool for the application you plan on using it for.
Motor
The motor will power the grinder and come in different wattages, determining the speed and strength of the tool output that you need.
For instance, high-power motors are suitable for heavy-duty grinders and demanding tasks, while lighter tasks can be handled by grinders with lower power ratings, for example.
Guards and Shields
Essential for safety, the guards protect you from flying debris or sparks during their operation.
Here, you always want to ensure that the grinder's guard is properly installed before you use it.
Handle and Controls
These tend to be ergonomically designed to help you handle and control the tool, helping to reduce your overall fatigue during prolonged use.
Speed controls here also allow for adjusting the grinder’s RPM based on the task at hand, all while giving you greater precision and safety at the same time.
Power Source
Grinders can be corded or cordless.
Cordless grinders, powered by batteries such as 18V Li-Ion batteries, offer you greater portability and ease of use.
Here brands like DeWALT and Makita can also offer you brushless motor cordless grinders, which give you longer runtime and increased efficiency as a result.
18V XR Technology
Many cordless grinders can also feature 18V XR technology, which provides you extended runtime and consistent power output - making them ideal for heavy-duty tasks in areas without direct power access.
Brushless Motor
Grinders with a brushless motor are also more efficient than ones without, giving you higher power, longer battery life, and reduced maintenance compared to more traditional motors.
Variable Speed Control
Variable speed control then allows you to adjust the RPM (Revolutions Per Minute) based on the task at hand, giving you greater control for different materials and applications as a result.
Quick-Change Disc System
Many grinders also come with a quick-change disc system, allowing you to swap out your grinding discs quickly and easily - increasing your efficiency while simultaneously reducing your downtime at the same time.
Ergonomic Handle Design
Grinders with ergonomic handles offer you better comfort and control, reducing user fatigue during long tasks and improving precision and safety.
Anti-Kickback Protection
Anti-kickback protection then helps to reduce the risk of sudden movements if the grinder catches or binds, providing you with a safer operation as a result - especially in cutting and grinding.
Dust Ejection System
A dust ejection system can also be included that helps keep dust and debris out of the grinder's internal components - prolonging the tool's life and improving your performance at the same time.
Spindle Locks
The spindle lock feature then makes it easier to change wheels or discs securely, improving your ease when using the tool and ensuring that you get a firm attachment during operation as well.
Adjustable Guards
An adjustable guard then allows you to reposition the guard for better protection against sparks and debris, giving you a lot of flexibility based on the task.
Overload Protection
Overload protection safeguards the motor by shutting it down if it starts to overheat - which prevents damage and extends the tool's lifespan as a result.
How Do Grinders Work?
Grinders rely on an abrasive process to remove material from the surface of a workpiece.
The high-speed rotation of the grinding wheel or disc creates friction, which chips away at the material being worked on.
Then, depending on the type of grinder and the abrasive material being used, the tool can perform various tasks, such as cutting, grinding, polishing, and even sanding for instance.
Then, different types of abrasives are used in grinding, ranging from aluminium oxide (for general-purpose grinding) to diamond-coated discs for tougher materials like stone or stainless steel.
Please note That the choice of disc size and material will affect the grinder's performance and suitability for specific tasks.
Choosing the Right Grinder For You
As you can see, selecting the right grinder involves considering several factors.
Consequently, some of these include, for instance:
Type of Task
First you want to identify the primary tasks you need the grinder for.
Cutting discs are suitable for cutting tasks, while grinding wheels are better for material removal, and for precision work, a die grinder or rotary tool might be more appropriate for you here.
Power Supply
You next want to decide between corded and cordless grinders.
Corded angle grinders offer you that consistent power, making them suitable for heavy-duty tasks, whereas cordless grinders, such as the DeWALT DCG418N, offer you more portability and are ideal for jobs where access to power is limited.
Disc Size
Next, you want to select the disc size or diameter as this affects the depth of cut and the area of material that can be removed.
Common disc sizes here include 115mm, 125mm, and 230mm, for example.
Larger discs are also suitable for heavy-duty tasks, while smaller discs are better for precision work we should note.
Motor Power
The motor's wattage will also determine the grinder's power and speed.
For instance, here, high-power grinders are more suitable for heavy-duty applications, while lower-power grinders are adequate for lighter tasks, for example.
Brand and Quality
You also want to consider investing in top brands like Bosch Professional, Makita, DeWALT, and Einhell Power X-Change, as these brands can give you a lot of reliability, performance, and access to repair services and customer support along with good brand warranties as well.
Safety Tips for Using Grinders
Grinders are powerful tools that can be dangerous if not used properly.
Consequently, in this part of the guide, we will look at some safety tips that you should consider to get the best out of your grinder as safely as possible.
For certain tasks, a face shield may also be necessary to protect against flying debris in line with your risk assessments.
Check the Tool Before Use
You also want to carefully inspect the grinder for any damage or wear, especially the grinding wheel or cutting disc, before you start using it.
Here, for instance, you want to ensure that the disc is appropriate for the material and that it's securely attached.
By failing to do so can lead to a bad finish or lead to more damage to the tool, or be breach of your safety processes, for example.
Use Guards and Shields
Never remove the grinder's guard, as this is designed to protect you from sparks and debris, and you want to make sure it is properly adjusted and in place before operating the tool as well - with the power turned off.
Secure the Workpiece
You also want to make sure that you ensure that the material you are working on is securely clamped or held in place to prevent it from moving due to use.
This then prevents movement that could lead to accidents from occuring.
Avoid Kickback
Be cautious of the grinder's position and angle to prevent any kickback from occurring - which can occur if the disc catches on the material, for example.
Accessories and Additional Tools
A grinder can also be improved with the right accessories for it.
Here, for example, you can easily find:
Extra Batteries & Chargers
For cordless grinders, having spare batteries and a reliable charger ensures that you can work uninterrupted for longer.
You should also consider investing in high-capacity batteries for longer runtimes as well.
Multi-Tools
Multi-tools and rotary tools also complement grinders by handling tasks that require more precision - such as engraving or detail sanding for example.
Diamond Blades
For cutting hard materials like concrete, stone, or stainless steel, diamond blades offer you improved performance and durability from your cutting discs.
Air Grinders
Air grinders are then powered by compressed air and are ideal for tasks that require high speed and precision.
These, for instance, are commonly used in automotive repair and metal fabrication jobs for example.
Need Help? Expert Advice and Customer Service
If you are still unsure about which grinder to choose or need assistance with your tool kit, don't hesitate to seek expert advice.
So, whether you need help selecting a flathead angle grinder or advice on which grinder is right for you, we are here to assist you.
How to Select The Grinding Tool Overall
As you can see, grinders and grinder tools are indispensable in a variety of settings, from professional metal fabrication jobs to home DIY projects.
Consequently, we hope by now that you understand the different types of grinders, their applications, and how to use them safely to help you select the right tool for your tasks.
So, whether you need a high-power brushless cordless angle grinder for heavy-duty work or a lightweight grinder for precision tasks, there really is a grinder tool suited to your exact needs.
Furthermore, investing in quality tools from reputable brands will also help you when it comes to reliability and performance. But also remember to consider factors like the power supply you will need, the disc size, and the nature of your tasks when choosing your grinder.
Lastly, always prioritise safety by following proper usage guidelines, remaining in line with your own risk assessments, and wearing appropriate protective gear.
As with the right grinder in your toolkit, you will be well-equipped to tackle a wide range of projects with efficiency and precision, and remember, if you are unsure, we are here to support you.
Contact Customer Support
If you are still not sure which grinder tool is right for you or you need help, then please contact our team, and we will be happy to help you understand which ones are perfect for you and your team.
Standard Delivery Information
We have also extended our delivery service and ordering hours to offer you next working day delivery, along with Click & Collect, making your shipping experience even easier.
Place your order online by 7 p.m. and choose the delivery charge that suits you best to ensure the timely, UK mainland hassle-free delivery of your products.
Standard next-day delivery is also available for all products ordered within the specified time, with free shipping for certain items as well.
Who Is MSC Direct?
Here at MSC Industrial Supply Co., we are a leading supplier of industrial tools, equipment, and maintenance supplies across the United Kingdom and can also offer you trade accounts, along with a wide range of inserts in our product range above.
We also serve a wide range of industries, from manufacturing and engineering to maintenance and beyond.
Consequently, our outstanding customer service and expert technical team, fast delivery times, and technical support make us a trusted partner for all your business needs as a result.