Carbide Drills

Carbide Drill Bits Range Explored

Definition: Carbide drill bits are very hard and durable, which are made from tungsten carbide, a ultra hard material that can drill through the toughest materials. As a result, they are designed for drilling into hard materials like metal, concrete, ceramics.. Because of their extreme hardness, they stay sharp for a long time and can drill at high speeds without wearing down quickly. As a result, carbide drill bits are often used when precision and durability are really important, making them very popular for professional work and heavy-duty tasks, for instance.

Materials Carbide Drill Bits Are Suitable for Use On

Carbide drill bits have become a cornerstone in modern machining and manufacturing, especially when it comes to working with the hardest materials.

Workpiece materials suitable for carbide drills consist of:

  • Alloy Steels
  • Aluminum
  • Brass
  • Bronze
  • Cast Iron
  • Carbon Steels
  • Ceramic Tile
  • Composite Materials
  • Concrete
  • Fiberglass
  • Hardwood
  • Hardened Steel
  • Inconel
  • Masonry
  • Mild Steel
  • Nickel Alloys
  • Plexiglass
  • Stainless Steel
  • Tool Steel
  • Titanium Alloys

MSC Edge 5mm 5xD Carbide TiAlN Coated Drill With Through Coolant

Ability to Cut Through Tough Materials with Precision

Known for their hardness and ability to cut through tough materials with precision, these drill bits are pretty much indispensable across various industries, from automotive manufacturing to aerospace engineering alike.

Crafted from a composition, of cobalt and tungsten tungsten carbide drill bits offer you a distinct advantage over traditional high-speed steel HSS drills, making them the preferred choice for professionals who need high-performance tools that are both durable and efficient.

How Carbide Drill Bits Came About

The journey of drill bits spans centuries, with early versions made from softer metals that could not withstand the demands of modern manufacturing.

Consequently, the advent of carbide technology marked a significant leap forward, literally revolutionising drilling processes by introducing carbide drill bits that really can offer unmatched efficiency and extended service life way beyond those that came before, allowing precision drilling, from seasoned professionals to DIY enthusiasts to occur a lot more easily as a result.

Types of Carbide Drill Bits

Drill bits come in various forms, each tailored to specific applications and materials.

While high-speed steel(HSS) drill bits are popular due to their affordability and adaptability, they can fall short compared to carbide drill bits. This is in terms of their extreme hardness, especially in high-demand environments.

As a result, Carbide drill bits are available in different variations, each designed more to serve distinct purposes, such as for instance:

Dormer R100 1.6mm Uncoated Solid Carbide Jobber Drill

Solid Carbide Drill Bits

Made from carbide, these drill bits offer you unparalleled hardness and wear resistance, making them ideal for high-speed drilling in hard materials like stainless steel, titanium alloys, and tool steel especially.

These precision drill bits are also perfect for applications requiring accuracy and longevity, such as in the aerospace and automotive industries for instance.

Carbide-Tipped Drill Bits

These types of bits combine a high-speed steel shank with carbide tips, offering you the toughness of steel but with the cutting performance of carbide.

As a result, they can be more cheaper than solid carbide bits, and they are commonly used in applications involving wood, masonry, and multi-material drilling on the whole.

Carbide-tipped multi-purpose drill bits are also adaptable enough to handle tasks such as wood, steel, stone and ceramic tiles.

Carbide Centre Drill Bits

Carbide centre drill bits are generally used on metal working lathes to create a small pilot hole on the end face of a long slender bar to locate a supporting tailstock.

These are then ideal for creating accurate pilot holes in hard materials like stainless steel, which then, in turn, ensures that you get a clean, centred drilling experience as an end result.

Jobber Carbide Drill Bits

Jobber carbide drill bits are then adaptable bits, providing you with reliable performance in various materials.

For instance, their longer length allows for deeper drilling, while the carbide composition ensures they have the strength and extended tool life in tough applications as well.

Micro Carbide Drill Bits

Microcarbide drill bits are then perfect for small accurate, detailed work, especially in electronics and precision engineering.

This is due to their small diameters, allowing for drilling tiny holes in hard materials with high accuracy and with minimal breakage occurring due to their design as well.

Interstate 0.6mm Carbide Uncoated Micro Drill

NC Carbide Spot Drill Bits

NC carbide spot drill bits then create precise, shallow indentations, ensuring positional accuracy before drilling can then start.

These prevent the main drill bit from then wandering, making them essential for precision work on hard surfaces, like tool steel, especially.

Straight Flute Carbide Drill Bits

Straight flute carbide drill bits then excel in drilling more brittle materials like ceramics or plastics.

This is then due to their design, which minimises chipping and cracking, helping to ensure that smooth, clean holes in hard or non-metallic materials can then occur.

Carbide Stub Drill Bits

Carbide Stub Drill Bits are short and rigid, providing excellent positional control and stability.

These are ideal for shallow drilling through thin plates for instance in any workpiece materials, as there is no flex or breakage, giving you good quality precise holes, in turn giving you more consistent results.

Three Flute Carbide Drill Bits

Three flute carbide drill bits then offer you a balanced design for efficient material removal and smoother holes on the whole.

This, in turn, makes them ideal for high-speed drilling in metals, as they provide you with an enhanced chip evacuation - which helps to reduce heat buildup during drilling and extends the drill bits' life as a result.

Dormer 8mm Solid Carbide 120° Spotting Drill

How Are High-Quality Carbide Drill Bits Manufactured?

The production of high-quality carbide drill bits is a process that begins with a selection of premium raw materials like tungsten carbide and cobalt in a powderd form and then compressed in very high pressure in dies, this is known as a sintering process, they are then put into a ultra high temperature oven for many hours until the power solidifies, this is then referred to as cemented carbide.

Tungsten Carbide Powder

For instance, Tungsten carbide powder can be compacted into the desired shape using powder metallurgy.

Sintering

This is followed by sintering, where the compacted powder is heated to bond the particles together without melting them.

Final machining

After sintering, the drill bits undergo final machining, and it is at this stage that they are often coated with protective layers, which can then enhance their tool life and performance which allows them to perform better when cutting different metals.

Retain Their Cutting Edges

This process then ensures that carbide drill bits retain their cutting edges while they perform exceptionally well under high temperatures.

Advantagous Properties of Carbide Drill Bits

Carbide drill bits are celebrated for their hardness, which can exceed that of most other materials in this field.

Remain Sharp

This characteristic allows them to retain a sharp cutting edge even under extreme conditions - including high-speed operations and high temperatures.

High Heat Resistance

Their heat resistance then further enhances their ability to drill through tough materials like hard steel and mild steel, all without losing their efficiency while they do so.

Strength

Carbide drill bits also last significantly longer than other types of drills, such as HSS twist drill bits, while reducing the need for frequent replacements.

Precision

Their sharp cutting edge ensures that clean, accurate holes can be drilled, which is crucial in precision engineering.

Hertel TiAlN Coated Solid Carbide Stub Drills - Metric

Adaptability

Capable of handling a wide range of materials, including hardened steel, carbon steels, titanium alloys, and composites, to name a few.

High Performance

These bits are also designed for heavy-duty use, making them ideal for drilling applications that require consistent, high-quality results.

Application Uses for Carbide Drill Bits

Carbide drill bits are pretty much indispensable in industries where precision, durability, and strength are pretty much non-negotiable.

Automotive

For instance, in the automotive sector, carbide drills are used to drill through tough alloys and hard steels, ensuring that components meet exacting standards and specifications as a result.

Aerospace

In aerospace, the ability to cut through high-strength materials like titanium, and nickel alloys with minimal wear makes carbide drill bits a preferred choice.

Oil & Gas

Additionally, the oil and gas industry can also rely on these bits as well.

Everyday General Purpose Applications

Beyond industrial applications, carbide drill bits are also essential in everyday tasks.

For example, carbide tipped jobber drills and centre drills are commonly used in workshops for a variety of materials, including mild steel and carbon steel.

Multi-material drill bits and tile drill bits are more adaptable tools for both professional tradespeople and DIY enthusiasts, and they are capable of drilling through ceramic tile, wood, and metal with ease.

How to Select the Right Carbide Drill Bit for Your Needs?

Choosing the correct carbide drill bit for a specific application requires careful consideration of several factors, including the workpiece material to be drilled, the desired hole diameter and depth of the hole, for instance.

Type of Drill Bit

The flute design, point angle, flute type and shank type (such as straight, weldon or whistle notch shank) also play critical roles in enhancing their performance, especially in deep hole drilling or when working with multi-materials especially.

Material Compatibility

You want to ensure the carbide drill bit is also suitable for the material you are drilling, whether it is tool steel, mild steel, or titanium alloys.

Coatings

Coatings like Titanium Nitride (TiN) or Aluminium Titanium Nitride AlTiN can also really enhance their durability and cutting efficiency - especially in heavy-duty applications as well.

Best Practices When Using Carbide Drill Bits

Using carbide drill bits effectively requires adherence to proper cutting techniques.

For instance maintaining the correct speed and feed rate is crucial to prevent drill bit breakage while also ensuring that you get a stable drilling process as well.

Cooling and Lubrication

Cooling and lubrication are also essential, as they help dissipate heat and reduce friction, prolonging the drill bit's life.

Speed and Feed Rates

You also want to adjust the speed and feed rates based on material and drill bit size to avoid excessive heat buildup - especially when using carbide drill bits on hard steels especially.

Cooling

Where possible, you want to use appropriate coolants or lubricants during drilling, particularly when drilling stainless steel or alloy steels.

Avoiding Mistakes

Common errors like applying too much pressure or entering the material at an incorrect angle can lead to premature drill bit failure and also a bad surface finish.

Consequently, you want to always ensure proper alignment and stability, especially when using machines, power tools, or hand tools.

Maintenance and Care of Carbide Drill Bits

Proper maintenance can easily extend the lifespan of your carbide drill bits as well all while helping to ensure that you get a consistent performance.

Then, after each use, you want to clean the drill bits to remove debris and store them in a dry, safe place to prevent damage.

Due to their hardness and accuracy requirements, re-sharpening carbide drill bits requires very specialised CNC grinding machines and professional services, to prolong the life of these drills once they become blunt.

Cleaning

When cleaning you want to remove chips and residue after each use.

Storage

Ideally, you want to keep bits in a protective case, such as a drill set box, to avoid chipping and getting lost.

Inspection

You also want to regularly check for signs of wear or damage, particularly on the cutting edges and shank. If found you want to consider replacing them

ZCC-CT 3.6mm 3-Flute Carbide Uncoated Drill

Safety Considerations When Using Carbide Drill Bits

Safety is key when working with carbide drill bits, especially given the high speeds and forces involved.

Consequently, you want to always wear proper Personal Protective Equipment (PPE), such as safety glasses, safety gloves, and hearing protection.

These can then help you to ensure that the bit is securely fastened and the workpiece is stable, which will also help prevent accidents from occurring.

PPE

Always wear appropriate gear to protect against debris and noise, particularly when using power tools or hand tools.

Secure Workpieces

Furthermore, you want to ensure the material being drilled is firmly clamped to avoid any movement, especially when working with a hinge cutter or core drill bit.

Drill Bit Handling

You also want to handle carbide drill bits carefully to avoid chipping or breaking them, due to carbide being very hard it also makes them very brittle.

Related Products and Power Tool Accessories

In addition to carbide drill bits, we offer a comprehensive selection of power tool accessories and related products.

So, whether you need a cobalt drill for extra durability, a masonry drill bit set for your construction needs, or a carbide drill bit for specialised applications, our extensive inventory ensures that you’ll find the right tools for any job.

Customer Support and Services

Our customer support team is also here to assist you with any questions or concerns you may have about our products.

Whether you are looking to set up a trade account, need advice on selecting the right carbide drill bits for stainless steel, or want information on day despatch services, we are dedicated to providing you with exceptional service.

So contact us today to learn more about our products and how we can help you achieve the best results in your projects.

MSC Direct's team

Delivery

We have extended our ordering hours and can offer you 'next working day' delivery to simplify your shipping experience.

Choose the delivery option that best suits your needs, and ensure your products arrive on time without hassle by placing your order online by 7 p.m.

Your products will then arrive the next day delivery as standard.

Who is MSC Direct?

Here at MSC Industrial Supply Co., we are a leading supplier of industrial tools, equipment, and maintenance supplies in the UK.

Consequently, we offer a wide range of products, including cutting tools, abrasives, power tools, and safety equipment, to name a small selection of our offering.

Consequently, we can cater to various industries such as manufacturing, engineering, and maintenance, along with many more.

Known for our exceptional customer service, we can provide you with very fast delivery and technical support, making us a trusted partner for your business.

Our website also features an extensive product catalogue of over 200,000's products and resources for engineering solutions. Consequently, we are here to help our customers find the right tools and equipment for their needs and applications, so give us a call if you are not sure. We are here to help.